(0)| 3/17/2008 5:54 PM | |
|
Posts: 1611 Rating:
|
Hi, for the problem with the "Loader" look to this FAQ (it is for ProTool but it should be the same for flexible). -> http://support.automation.siemens.com/WW/view/en/15178055 For your other problem i did not realy have an idea. Maybe you should contact the customer support regards, |
| 3/19/2008 2:22 PM | |
|
Posts: 1611 Rating:
|
Hi, do you want to start the flexible runtime project using autostart? Create a shortcut from the *.fwx data. Put this short cut to the desktop (Maybe you give the symbol a nother name) Put this short cut from the desktop to "Start > Programs > Startup" (Drag&Drop) After you start the pc, the project will be start. -> Look to the attachment, there are two screen shots. regards, AttachmentAutostart.zip (183 Downloads) |
Follow us on