6/6/2011 2:43 PM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, this FAQ is very helpful: How are tags and alarms logged in WinCC flexible? The limitations about the max. entries per log can be found in the flexible help (systemlimits). best regards. |
6/7/2011 9:48 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
You can use a MMC-card or a USB-stick for logging at a MP277. The internal memory can`t be used for the logging (would reduce the lifetime of the panel). This faq is also intersting for you in this case i think: Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have? |
4/25/2016 10:31 AM | |
Joined: 5/29/2012 Last visit: 9/3/2025 Posts: 18 Rating:
|
Can this hostorical data being transfered via network? |
4/25/2016 12:17 PM | |
Joined: 5/28/2008 Last visit: 8/31/2025 Posts: 4522 Rating:
|
Hello, I think yes. I have never did but in the attachement of the following link, read sections from 4.2.3 WinCC flexible 2005: Accessing a Panel via an HTML Page Supported by Sm@rtAccess |
Ayman Elotaify |
|
Follow us on