(0)| 4/28/2016 6:51 PM | |
|
Posts: 8 Rating:
|
Hello,
"The eWON remote maintenance solution for the MPI and Profibus devices is based on the use of a transparent gateway between the ISOTCP and the MPI/Profibus protocols. This solution has the advantage that it is transparent for the Siemens software and the involved PLC. A drawback of this solution is that the Operator Panels cannot be accessed from remote on their MPI or Profibus interfaces, because the transparent gateway cannot be used for these devices. So to make a remote maintenance on an Operator Panel the Ethernet interface of the OP has to be used OR use eVCOM to make remote maintenance of Operator Panel." I've tried the eVCOM method, but with no luck. I get stuck on page 16 of this manual. There is no "Local connection" tab and therefore no way to specify a COM port - according to the Help documentation, the Local Connection tap is a "32-bit operating system only" thing (not sure why that makes a difference). Everything seems to fall apart after that point, and I haven't find another way of doing this. Any ideas? |
| 4/28/2016 8:53 PM | |
|
Joined: 12/16/2012 Last visit: 9/8/2025 Posts: 655 Rating:
|
Hi! You should try to reinstall the PC MPI adapter driver. |
Follow us on