(0)| 4/8/2008 3:13 PM | |
|
Joined: 4/24/2006 Last visit: 1/14/2026 Posts: 9105 Rating:
|
Hi, Yes, when you have WinCC flexible 2007, you get version 1.3. You have WinCC flexible 2005 + sp1, so you can only use version 1.2 You will have to perform an OS update, see link: http://support.automation.siemens.com/WW/view/en/19701610 Then you can download your project to OP73. Best regards, Wizard |
| 4/8/2008 3:28 PM | |
|
Posts: 15 Rating:
|
Dear Wizard, Let me imagine your answer first. Is it you mean that: a) If I have WinCC Flex 2007, I do not have to do the OS update. Just simple select the v1.3. b) If I have WinCC Flex 2005 + SP1, I have to do the OS update using serial PC/PPI Multimaster cable. And also have the image file of that v1.3. |
Follow us on