4/7/2008 3:18 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating:
|
The attached page explains how to connect braking-units in parallel. Do not mix up max. braking-power and P20-value. You can use the P20-value only for 20 sec; then there must be a break of 70 sec. P20 must be smaller than 2,4 * rated power of drive. If you constant braking-poweris 250 kW, it would be better to use a RRU or AFE. AttachmentSeiten aus ba_bremsein_komp_e.pdf (442 Downloads) |
4/11/2008 7:03 AM | |
Joined: 9/20/2006 Last visit: 8/1/2025 Posts: 307 Rating:
|
attached findthe braking unit manual. AttachmentBraking units DA1 type.pdf (490 Downloads) |
Follow us on