(0)| 8/19/2016 12:58 PM | |
|
Posts: 4 Rating:
|
Hello all, Today, I have Two V90-PN Connect to CPU-1215C. ------------------------------------------------------------------------------------------------------ When I only use One V90-PN with SINA_PARA(FB 286) to read parameter is OK, but today I want to read Two V90-PN 's parameter, but I get error. 1. When I click "Rename and paste objects", the old one SINA_PARA will be Red. about ERROR. 2. When I click "Replace existing objects and move to this location" , compile will be Error. because there have Two FB286 in CPU at same time. ------------------------------------------------------------------------------------------------------
Best Regards, ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/19/2016 1:39:50 PMNew subject after splitting |
|
This contribution was helpful to
|
|
Follow us on