(0)| 4/17/2008 12:15 PM | |
|
Posts: 5 Rating:
|
i faced problems, as i was working on S7-300 System, during downloading program to HMI via MPI, connection not established between laptop and HMI (TP 277). |
| 4/17/2008 9:44 PM | |
|
Joined: 4/6/2006 Last visit: 11/21/2025 Posts: 604 Rating:
|
Hello, You dont mentioned which cable you use to get a connection, is it a PC Adapter? If it is this could be the problem. What transfer options are available in the various operator panels? The document tells the following about MPI:
But I think you will be able to get online when you are connected to the PLC and the PLC is connected with the same cable to the panel. |
|
Best regards, |
|
Follow us on