(1)| 6/10/2016 10:32 AM | |
|
Posts: 4757 Rating:
|
New question published by kzsolt2 is split to a separate thread with the subject LOGO!Soft Comfort V8, export logo to bin error. Best regards |
| 9/8/2016 8:57 AM | |
|
Joined: 4/16/2014 Last visit: 10/28/2024 Posts: 6 Rating:
|
Thanks for this workaround! I will try it the next time. But what about the bugs with the blocks not lining up correctly in FBD. It's like the blocks snap differently to the background dots sometime when you open the application. You can have the exact same block next to each other but they wont line up correctly. Yes you can use "align" but that's just a tedious workaround.
Add Block1, rename it "long name" Add Block2 Connect them and split it (separate) I like to have the diagrams tidy and compact but the second end of the separated connection behaves very strange if it's too close to the second block (Block2) Also when you try to move the end of the separated connection just one pixel, it lags like crazy and jumps many pixels. If you do the same while having the end further from the second block you can move it pixel by pixel without a problem. Uploaded an example. Not sure if you can see the problem or if it's machine specific. In LOGO!Soft 7 there wasn't this problem from what I can recall. I also find it strange that we are using 8.0.0 from 2014. Attachmentseparated connection bug.zip (513 Downloads) |
| 9/19/2016 9:23 AM | |
|
Posts: 4757 Rating:
|
New question published by amrelhajali is split to a separate thread with the subject luf file to update from 7.15 to 8. Best regards |
Follow us on