(0)| 6/17/2016 9:45 PM | |
|
Posts: 1 Rating:
|
Hello all, I have a 6ES7 416-3XR05-0AB0 CPU that failed to go to run mode after a hardware change (added a new device on the Profibus PA network). note that - the cup goes to run mode once I remove the new device. - I have already replaced the external memory. - all the necessary OBs are in place. - I tried to do it with only HW downloaded to the CPU and empty OBs. Module or submodule assignment not evaluated or evaluation aborted with errors (SDB 1,3,5,2X,9X) so I downloaded the same program in another CPU same type the problem persisted then I suspected the CPU type so I went and installed another type 414 CPU still the same. I tried many different things but no success. so I will rely appreciate your help on this issue as it's delaying our gold plant upgrade. thanks in advance, Hamma ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/20/2016 4:20:26 PMNew subject after splitting |
|
| 9/19/2016 11:09 PM | |
|
Posts: 18 Rating:
|
I have the same problem, and i've taken your advice, but it stil dose'nt work, it remains in stop mode. To move forward with the project i've made a HW config. in witch I inserted only one CPU and it works. But however when I download the redudant sistem i receive the same erors. It is to mentioned that i only have one fiber optic cable, and the other one is on the way. Best Regrads AttachmentDiagnose.txt (543 Downloads) |
Last edited by: RogerBRO at: 9/19/2016 11:19:21 PM |
|
| 9/20/2016 12:13 AM | |
|
Posts: 83 Rating:
|
please upload "diagnostic buffer" |
| 9/20/2016 2:11 PM | |
|
Posts: 18 Rating:
|
I've attached the diagnostic buffer.
AttachmentDiagnose.txt (553 Downloads) |
| 9/20/2016 8:10 PM | |
|
Posts: 83 Rating:
|
check your simatic version same problem here Attachment3XR05.zip (569 Downloads) |
Last edited by: amr ali at: 9/20/2016 8:13:28 PM |
|
| 9/21/2016 8:43 AM | |
|
Posts: 18 Rating:
|
This is not the problem, because I have a new version of software. |
Follow us on