(0)| 9/19/2016 5:26 PM | |
|
Posts: 2 Rating:
|
Hai Everyone, I'm using CPU 412-5H PN/DP , my first CPU(rack 0) is going to run mode and if I turn it stop it the master LED is switching to the next CPU(rack1) but that CPU(rack1) is not going to RUN MODE , even the stop mode LED also not glowing. CPU (rack 0) is going to run mode but in my pc hardware configuration the CPU is shown Shaded ,where the IM module is communicating but Y-LINK is not. Sugguest me what to please, I attached the the Snap of HW configuration ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/20/2016 12:28:28 PMNew subject after splitting |
|
| 9/20/2016 2:22 PM | |
|
Posts: 18 Rating:
|
Have you downloaded the program to the both memory card? PLC -> Download User Program To Memory Card |
Follow us on