(0)| 11/1/2016 6:42 AM | |
|
Posts: 124 Rating:
|
Hello Luna, Take a look. I don't know all KTP700 features, but there are eigh onscreen function keys. I have considered the use of them. The program has two options: 2 and 4 cicles. You can expand whenever you want. There are several things to implement: 1. Interlock: each new start depends on refreshing counters and choosing what cicle's number will be done. 2. Power loss: the carriage will be between the two limit switchies. Automatic mode will not act up. 3. Coil seals, thermal contact, etc. Something else, please ask. Regards. AttachmentAutomatic motor reversion with steps counters 31 10 2106.zip (199 Downloads) |
Follow us on