(0)| 11/5/2016 10:02 PM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36482 Rating:
|
I suspect that LSC V8.1 does not work flawlessly. For several projects I noticed, if the source program under V8.1 was created, that there are problems, if it with V8.0 opens and try the hardware change over. An 0BA8.Standard has been selected as hardware in the source file under V8.1. The error message "Failed to load the panel" comes up. When the message is acknowledged, different things happen, depending on the program. I have opened the program as V3 and set the first error. After that, the program had changed several times, deleted blocks and inserted UDFs. This is then the V6. In the simulation and in the real LOGO! 0BA8.Standard the programs works error free, but only the hardware can not select. AttachmentBug_LSC_V8.1.zip (277 Downloads) |
Last edited by: ixo65 at: 11/5/2016 10:04:32 PM |
|
This contribution was helpful to
|
|
Follow us on