(0)| 7/7/2016 6:47 AM | |
|
Posts: 15 Rating:
|
We have also problem in DP/PA couple. Why is the signal from the PA device intermittent? What should we do to correct this problem? See attached PDF for the setup. Hope to hear from you asap. ------------------------------------------------------------------------------------------ AttachmentReport.pdf (293 Downloads) |
Last edited by: Min_Moderator at: 7/7/2016 12:59:03 PMNew subject after splitting |
|
| 7/12/2016 10:44 AM | |
|
Posts: 15 Rating:
|
Hi Sir, Thanks for the reply. Attached is the screenshot of diagnostic buffer. |
| 7/18/2016 11:29 AM | |
|
Posts: 15 Rating:
|
Any suggestion? Thanks |
| 7/28/2016 5:25 AM | |
|
Posts: 15 Rating:
|
I really need an answer. Our project was delayed because of this issue. Hope you will help me.Thanks experts! Regards |
| 8/11/2016 4:34 AM | |
|
Posts: 15 Rating:
|
Help PLEASE? |
| 11/9/2016 2:51 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello KVOJ; In the following Word page I have extracted from the DP/PA coupler manul 2 elements that might be part of the problem. The most important one is the Profibus-DP bus speed: if you are using a DP/PA coupler (FDC 157) as a stand-alone unit, you do not need to configure it on the bus (only the PA instrument using its GSD file); however the bus speed of the DP must be brought down to 45,45 kBaud. What are your present settings (right-click on the Profibus line of the HWConfiguration editor, and open the Bus Parameters tab)? In any case I suggest you review chapter 7 of the manual (the link is attached to the document), it describes the basics of commissioning a DP/PA coupler. You should find a good number of hints for your application. Hope this helps, Daniel Chartier AttachmentSIMATIC Bus links DP_PA coupler.docx (266 Downloads) |
Last edited by: dchartier at: 11/9/2016 3:10:45 PM |
|
Follow us on