1/29/2013 7:21 AM | |
Joined: 3/31/2012 Last visit: 10/15/2024 Posts: 52 Rating:
|
Yes S7 417 5H PLC Compatible With PCS7 V7.1 +SP4. But You need to Upgrade Your Step7V5.5 to Step 7 V 5.5 SP2 and SIMATIC_STEP7_V55_SP2_HF1. |
1/29/2013 10:10 AM | |
Joined: 10/3/2007 Last visit: 6/25/2024 Posts: 188 Rating:
|
It is not allowed to upgrade a step 7 version within PCS7, this will break the relationship between the components PCS7 that are part of PCS7. You can only upgrade PCS7 itself to have a newer version of step 7. That being said, you can allways usenewerCPU's within PCS7 as they are downward compatible. This means you can configure a firmware version 4.5 CPU in HW config but really insert a FW V6 CPU. This way you cannont use the functionality of the new CPU (eg the Profinet ports) but you will be able to take advantage of the faster execution speed. Hope this helps, David |
12/12/2016 5:01 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
New question published by AEG Systems is split to a separate thread with the subject HSP to see 417-5H family in Hardware Catalog?. Best regards |
Follow us on