12/22/2016 6:57 PM | |
Posts: 6 Rating:
|
How to set input bit high I0.1 using button and tag in wincc directly without using M OR DB ETC. I succeed it by using setbit M 0.1 but cant do it directly. |
12/22/2016 9:09 PM | |
Posts: 6 Rating:
|
i want to high I0.1 using external tag so that i can program existing physical switch with in HMI. |
Last edited by: uu0sa at: 12/22/2016 9:09:55 PM |
|
12/22/2016 10:07 PM | |
Posts: 6 Rating:
|
i mean that i can design input button to the address i0.1 so tell me how to tag |
12/23/2016 12:54 PM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16447 Rating:
|
Hello uu0sa you could only set HMI Tags. Not directly data in the PLC. So you have to use a connection to the PLC and create a HMI tag with an Adress -> so you could set it. So this is a quite basic topic, perhaps this one helps you: https://support.industry.siemens.com/cs/ww/en/view/24109937 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on