(0)| 1/18/2017 6:51 PM | |
|
Posts: 2 Rating:
|
****************************** Thanks in advance. PS: I do attach both files. Attachmentfiles.zip (285 Downloads) |
| 1/28/2017 9:57 PM | |
|
Joined: 11/14/2016 Last visit: 3/5/2024 Posts: 218 Rating:
|
Hi I just copied your setup to network project and then it should work, have not checked about the IP settings. Do not set the Logos up as separate ones but together in a network project from the start. Split the window into two screens and it will be much easier. There are some good examples for download available on the support websites. AttachmentProject.lnp.zip (292 Downloads) |
| 1/30/2017 8:42 AM | |
|
Posts: 2930 Rating:
|
Hi, post your program so we can have a check. |
Follow us on