(0)| 2/28/2017 10:33 AM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Dear User, All H CPUs can be used as standard S7-400 stations.It is easy while selecting hardware if you implement the project manually.An S7-400H station is expensive due to extra set of hardware that are required(rack,SYNC.Module and FO link ,Redundant slaves and an extra CPU.At the following link, you can fine out more about the software package and details of hardware accessories: 6ES7410-5HN08-0AB0(PCS 7 CPU410 SMART F. S7-400/S7-400H)I hope it helps, hdhosseini |
This contribution was helpful to
|
|
Follow us on