(0)| 3/31/2017 7:41 PM | |
|
Joined: 12/18/2014 Last visit: 1/15/2026 Posts: 36459 Rating:
|
To 1.) So it is. Download via LSC loads only the last CSV file. To 2.) This is also correct. It saves only 50 CSV files to the SD card. Each file contains a maximum of 20,000 line entries. To 3.) There must be a pause of 500 ms between each log operation. If the time is not reached, the system will not be logged. The appendix contains an extract from the current manual. AttachmentLOGO! 8 Soft manual 0BA8 2016_07 (FS4) pages 273+274.pdf (204 Downloads) |
This contribution was helpful to
|
|
| 4/1/2017 4:16 AM | |
|
Joined: 12/18/2014 Last visit: 1/15/2026 Posts: 36459 Rating:
|
No. There's no way. |
This contribution was helpful to
|
|
Follow us on