(0)| 4/30/2017 9:24 AM | |
|
Posts: 1 Rating:
|
Can I connect ET200M IO's with S7-400H controller on profinet by using Profibus to profinet converter? The details of ET200M IO's and Profinet to Profibus converter is as follow. ET200M IO's: IM153-2 | IM153-2 | SM | SM | SM | SM | SM | SM Profibus to Profinet Converter: MGate™ 5102-PBM-PN Series ET200M IO's are installed in the remote rack. Arachitecture is attached for reference.
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/3/2017 9:57:13 AMNew subject after splitting |
|
Follow us on