5/9/2017 10:10 AM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello HIM61, I assume, the setpoint comes via PLC. So setting p353 from e.g. 1500rpm to 2000rpm increases the speed if 4000h is sent by the plc. Some common information: The link to the compendium Masterdrives VC 3.4:http://support.automation.siemens.com/WW/view/en/13472409 The link to the commissioning tool DriveMonitor:http://support.automation.siemens.com/WW/view/en/11769381 |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on