(0)| 5/30/2017 4:43 AM | |
|
Posts: 12 Rating:
|
Hi, I have attached Diagnostic Messages (Master PLC which is showing External Fault) Regards Prakash AttachmentDiagnose_Master.txt (297 Downloads) |
Last edited by: The Helping Hand at: 5/30/2017 10:05:25 AMRemoved personal information |
|
| 6/5/2017 1:28 PM | |
|
Posts: 623 Rating:
|
Hi Prakash_Chennai, This fault is due to DP slaves which does not get initialised/configured during PLC startup. U should again perform Master-slave changeover by putting PLC0 in stop mode. Now if CPU1 is without external fault, then the problem is with monitoring times 1. Finished message from modules 2. Transfer of parameters to modules[CPU properties-Startup. |
Follow us on