(0)| 6/30/2017 2:14 PM | |
|
Posts: 2 Rating:
|
Hello, I successfully connected a KTP 400 basic to a Siemens Logo8.FS4. Everything works fine with Network Signals and analog Signals to he KTP and Digital Signals from the KTP. One thing I could not figure out is how to Map a digital output from the Logo to the KTP. The problem is that I want to use the network output from the Logo to crate an event which illuminates a circle on the KTP screen when according to the status of an inductive sensor. I hooe someone can help me. ------------------------------------------------------------------------------------------ AttachmentLogo Tia.zip (416 Downloads) |
Last edited by: Jen_Moderator at: 6/30/2017 2:24:40 PMNew subject after splitting |
|
| 6/30/2017 2:35 PM | |
|
Joined: 12/18/2014 Last visit: 1/17/2026 Posts: 36470 Rating:
|
The state of digital outputs is determined by the operating system of the LOGO! In firmly allocated areas in the VM area. Example: AttachmentLOGO! 8 Soft Comfort Online-help 2016_07 (FS4) page 114.pdf (608 Downloads) |
Follow us on