(0)| 6/29/2017 9:30 AM | |
|
Posts: 531 Rating:
|
You should access the device via lan cable and search for it. Than you can set the name via a tool. like proneta or step 7. No need for prommer. |
| 6/30/2017 3:04 PM | |
|
Posts: 5521 Rating:
|
hi, if you insert an empty card into the device, the IP and the NameOfStaition will be written on the card. you can also use the function "device-change without Change-media". therefore you need to project the topology. following manual, chapter 4.4, describes it: SIMATIC PROFINET System Description hope this helps, regards, |
Follow us on