(0)| 7/7/2017 3:42 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello domdiz; The two modules you discuss are not the same at all: 6ES7132-1BH00-0XB0
ET200L, EL-BLOCK, 16DO, DC 24V, 0.5A 6ES7193-1CH10-0XA0 One is the electronics block for the ET 200L, it will be described by the number and type of I/Os it supports. The other is a terminal block on which the electronics block is mounted. The terminal block is not part of the Profibus configuration, so you will never find it in a Profibus catalog. So, what part do you actually need, the EL. Block or the Term. Block? Or both? I would go back to your Siemens rep. and ask for the price of this spare parts module (Siemens increases the price by a large percentage when the supplied part numbers are no longer produced). The spare parts will be available until 2022, as per Product Support, but pricing will go up as the final date approaches. Maybe you should think about selecting more up-to-date product lines: Which function successor modules can you use for the ET 200B, ET 200L and ET 200L-SC? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 7/7/2017 3:43:45 PM |
|
Follow us on