(0)| 7/19/2017 8:49 PM | |
|
Posts: 29 Rating:
|
Hey Guys, I'm trying to understand the difference between these two options: ET 200SP Open Controller and S7-1518-4 ODK . It looks to me that the ET 200SP is basically an industrial PC in ET200SP form factor running a soft PLC w/ the open controller package, however the S7-1518-4 is still a dediated PLC however it has the open controller package as well. Is this generally a correct understanding. Are they the same open package? Specifically, I'm interested in the Matlab coder package (shown here, I think?) which seems to utilize the open controller (at least for the ET 200SP). Is the Matlab package shown taking advantage of the same open controller package in these two controllers? Thanks, -Nate |
Follow us on