(2)| 7/19/2017 9:30 AM | |
|
Joined: 4/28/2017 Last visit: 12/6/2024 Posts: 149 Rating:
|
Dear Experts, I got new SIMATIC CPU 1215-DC-DC-DC With FW V4.2. I installed the Module on Existing line for Replacement. And, I Downloaded the Program to the CPU. There is no Error Occurred until i Download. After that, PLC Shows Error Indication in Module LED Indication. I used to Read the Online status. That time also PLC showed ERROR. I have attached the Screen Shots. Actually, In Online, CPU shows The Problem in HSC (High Speed Counter) Hardware or parameter Assignment. But,With My knowledge i verified everything.There is no Problem in Hardware Connection and parameter Assignment. I used the same program in old PLC. But, the Firmware version is different. "High Speed Counter" parameters are looking good. Kindly Help me To clear out the Problem. AttachmentSimatic_1200_CPU_Er.zip (312 Downloads) |
Last edited by: Sanakiyen at: 7/19/2017 9:35:20 AMLast edited by: Sanakiyen at: 7/20/2017 7:07:53 AMNote: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
Follow us on