4/4/2017 9:07 AM | |
Joined: 6/23/2016 Last visit: 5/9/2025 Posts: 16 Rating:
|
Thanks a lot for showing me the good rout. I've uninstalled PLCSIM, deleted "C:\ProgramData\Siemens\Automation\Portal V14" folder. Then I downloaded PLCSYM V14 SP1 from official site , not by updater. "Clear" install, reboot and everything works fine now :) P.S. When I go to "Help > Installed software" I see version V14 of PLCSIM, not V14 SP1. I could find that it is SP1 only by clicking "Detailed information about installed software", think it is some kind of "bug". |
4/10/2017 4:30 PM | |
Posts: 1 Rating:
|
have the same issue, siemens tell me to uninstall--->install PLC sim |
5/30/2017 12:12 PM | |
Joined: 4/12/2013 Last visit: 6/9/2022 Posts: 8 Rating:
|
Same thing worked for me! Thanks for the solution |
7/24/2017 7:49 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by KIKEUCHIJA is split to a separate thread with the subject Not able to start PLCSIM V14 in W10 . Best regards |
Follow us on