(0)| 7/17/2017 6:49 PM | |
|
Joined: 1/5/2015 Last visit: 2/6/2025 Posts: 108 Rating:
|
Thanks christophD, I have another question seince we are in this topic! In TIA portal V14 SP1 i am trying to connect two PLC's one master the other slave in which i have to transfer more then 4 words from master to save and viseversa ( the case with sinamics control and someother). Now under I-slave option i found out that i can make only one transfer and that from master to slave in 1byte length of data. What are there any options that would suit my needs? PS. in the master connection i have also some other slave devices such as sinamics g150, TP177B hmi and a PAC3200. ------------------------------------------------------------------------------------------ New question published by Dren Bejtullahi is split to a separate thread with the subjectCan make only one transfer and that from master to slave. Best regards |
Last edited by: Dren Bejtullahi at: 7/17/2017 6:52:52 PMLast edited by: Jen_Moderator at: 7/24/2017 8:52:34 AMNew subject after splitting Last edited by: Jen_Moderator at: 7/24/2017 8:54:46 AMInserted Information regarding new Topic |
|
Follow us on