(0)| 9/3/2017 8:53 AM | |
|
Posts: 1 Rating:
|
Dear Team , i want to Read 32 Hart Variables on An Single 6ES7 331-7TF01-0AB0 Hart Communication Module ,As in Hardware Configuration only 8 Hart Variables i can Configure , and i am reading only 8 Hart Variables , But As per My Requirements i need to Read 32 Hart Variables , so is it possible with the help of SFC58 and SFC 59 to read 32 HArt Variables on Single AI HART Module ???????? if possible than Please Share an Sample Project., it will be Helpful for me Thanks in Advance !!!!!!!!!! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/4/2017 9:24:12 AMNew subject after splitting |
|
| 9/7/2017 9:41 AM | |
|
Posts: 5521 Rating:
|
hi, thats not possible. See the manual, chapter 3.2.3: SIMATIC ET 200M distributed I/O device HART analog modules
hope this helps, regards,
|
Follow us on