(1)| 9/12/2017 12:26 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello Abdullah,
You still need synchronization modules and fiber optic patch cords.
No, You don't need any additional modules.
The A5E00267695-07 manual is not the latest. Check this one for Profinet IO configuration with H-systems.
No, Only ET200M. Keeping in mind the possibility to use ET200SP HA in the latest version of PCS7 with 410H CPUs, Best regards, H-H |
This contribution was helpful to
|
|
| 9/19/2017 11:34 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Thanks Ste_angioni. I stand corrected. You are absolutely correct regarding the ET200SP. Although it is neither mentioned in the 400H manual nor in Which PROFINET devices support media redundancy and which system redundancy?, it seems to be working. I've tested it within SIMATIC Manager's HW configuration and looks working It's also clearly mentioned in the Function expansions for ET 200SP interface and I/O modules.
Once again, thanks for the tip. Best regards, H-H |
Follow us on