12/5/2017 12:51 PM | |
Posts: 4 Rating: (0) |
Hello everybody, I’m trying to simulate a process at TIA Portal, it consists of a PLC S7-1500 1515-2 PN and a pc station running in PC. I want to link the ‘X’ status tag of a Step in the Graph program to an animation just to visualize a condition. I found an example of Siemens (Simatic STEP 7 Professional/Wincc Advanced V11 for Sample project Filling Station) and I executed the steps of the example but it’s not working, when the Step in the Graph is active nothing change in the animation. Could anyone tell me if it needs a configuration to work or it's not possible to do? Tia Portal V13; Wincc RT advanced. Thank, andredstrf. AttachmentSCREENSHOTS.zip (56 Downloads) |
Last edited by: andredstrf at: 12/5/2017 2:07:04 PM |
|
Follow us on