(0)| 1/10/2018 11:22 AM | |
|
Posts: 27 Rating:
|
Dear All, Recently I have performed many efforts to connect online with several s5-cpu, among these s5-100U, 155U, 947/947 with no result. To achieve this I utilized s5 software V 7.23 which is installed in a Windows 7 (Host) virtual environment (VM Ware) of Windows Xp Proffesional (Guest). In the hardware side I used a 6ES5734-1BD20 cable which I purchased from e-bay. Additionally a serial to USB adapter. The usb to serial coverter was tested with a loopback jumper within the environement (Short Circuiting Pins 2-3) of the Virtual Machine and it was working. Any effort though to connect to the PLCs fails due to error "Systen Error No, 0334". I read all the topics and solutions provided in this forum (regarding adjustment of serial port advanced settings) and I applied almost all of them but the problem remains. (1. https://support.industry.siemens.com/cs/ww/en/view/9072665 2. https://support.industry.siemens.com/cs/ww/en/view/18548070 ) Any possible suggestions to overcome this issue? |
Last edited by: Jen_Moderator at: 1/19/2018 12:04:19 PMInserted right links. |
|
Follow us on