(0)| 1/17/2018 6:59 PM | |
|
Posts: 1 Rating:
|
Hi, I am trying to connect Siprotec 7SD8021 via the pc PC manually and use the DIGSI to connect to the relay. For possible reasons, the program says; 1. The connection cable is not connected to the correct PC interface. 2. The connection cable is not connected to the correct device. 3. The device has not yet been initialized. 4. Parity or stop bit are not identical (for RS232/RS485). 5. The VD address has been changed. 6. The IP address is not correct (for PPP/Ethernet). I configured Digsi 4.91 and chose the PC ip address in the program too. What can I do to sort this out? taha taha ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/18/2018 11:18:47 AMNew subject after splitting |
|
Follow us on