(1)| 1/26/2018 9:14 PM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello Matwon; The manual you are refering to might be dated from 2008, this is teh version your document title points to ;you can check your own version on the cover page. ET 200M interfaces for Profinet were not as popular then as they are now. These days, when you talk of an ET 200M station, all Profibus and Profinet configurations are supported. For example, look at the following webpage from Siemens: http://w3.siemens.com/mcms/distributed-io/en/ip20-systems/et200m/pages/default.aspx DescriptionSIMATIC ET 200M is the modular I/O station for the control cabinet with high density-channel applications. Connection to PROFIBUS and PROFINET is achieved using interface modules – optionally for PROFIBUS also using fiber optic cables. The ET 200M can be used for standard as well as failsafe applications.Up to 12 multi-channel signal modules (e.g. 64 digital inputs) and function modules as well as S7-300 communications processors can be used as I/O modules – the interface to the process. ET 200M supports modules with expanded user data, e.g. HART modules with HART minor variables. I believe you can install and configure your HART modules without trepidation. Hope this helps, Daniel Chartier Edit: I have locate a manual on ET 200M HART I/O modules that describes the use of the Profinet network; it is dated 2011: et200m_hart_analog_modules_manual_en-US_en-US.pdf... Hope this helps, D.C. |
Last edited by: dchartier at: 1/26/2018 9:16:22 PMLast edited by: dchartier at: 1/26/2018 9:41:09 PMLast edited by: Jen_Moderator at: 1/29/2018 12:08:21 PMInserted right link. |
|
| 1/29/2018 4:08 PM | |
|
Joined: 5/24/2012 Last visit: 4/24/2025 Posts: 70 Rating:
|
Great! Thanks for the information Daniel |
Follow us on