(0)| 1/31/2018 7:33 AM | |
|
Posts: 8 Rating:
|
Dear Expert I want to upload the parameters of the SINAMICS drive on the Profibus PLC network via Ethernet using the STARTER (v4.5) software. The CPU used is 412-2 DP (v5.3) and CP is used type 443-1 (v2.1) which supports routing. The inverter unit is SINAMICS G120 with CU240E-2DP firmware control unit (v4.4) I am using SIMATIC S7 (v5.5 + SP2) software installation on a computer with Windows professional 7. I have followed some of the instructions contained in this forum, but I still can not access SINAMICS drives via Ethernet. Note: to upload drive MICROMASTER 440 (v2.1 and v2.1) I have tried and succeeded, Please help me for the problem I am facing, for the supporting picture is in the attachment. Thank you very much
AttachmentSCREEN SHOOT.zip (320 Downloads) |
| 1/31/2018 8:41 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice.
|
Follow us on