(0)| 2/20/2018 7:22 AM | |
|
Posts: 10 Rating:
|
Dear Experts, I had communicate between micro win S7 200 & Schneider HMI GXO 350 I can able to read write through HMI. its working fine. but I cant able to use double integer from HMI. example: I set the set point values via HMI. every time I can chose my set point. once I switch off the HMI the all set points goes to Zero. this is the issues I am facing now. suppose I selected the double integer from HMI, but the address not available in HMI that VD format. only having VW,VB,IO,IQ here I attached the screen short of HMI I hope you can understand my issues kindly suggest to proceed AttachmentDoc1.docx (379 Downloads) |
Follow us on