(0)| 4/10/2018 6:34 AM | |
|
Posts: 39 Rating:
|
I want to use a single modbus master (IM151-8F PN/DP) with 2 clients (Raspberry PI, and a Laptop). I have read here that (Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 PN-CPU as Modbus server) it may be possible using 2 different port numbers. I have tried calling MODBUSPN with different MODBUS_PARAM (each having a different port), but it does not seem to work. I can only make a connection once, and the other connection fails |
Last edited by: Jen_Moderator at: 4/10/2018 11:17:40 AMOptimized link. |
|
| 4/10/2018 10:59 AM | |
|
Posts: 5521 Rating:
|
hi, as Duris_I said, you need two different connections. That means you have to call the block with two different IDs and different Instance-DBs. regards, |
Follow us on