(1)| 4/16/2018 12:50 PM | |
|
Posts: 15 Rating:
|
Hey, Rana88! I search for Best oil lubricated air compressor and got some effective air compressor for you. I believe the 21 gallon Central Pneumatic air compressor from https://bestaircompressorstore.com/central-pneumatic-air-compressor-review/ will be the best choice for your want. It has a powerful 2.5 hp motor which is produces 125 psi max of pressure and able to deliver 5.8 CFM at 40 psi & 4.7 CFM at 90 psi of compressed air. This machine is also will be the perfect choice for the best portability to any place. Its two wheels and one handle strongly help you for transportation. Thank you |
This contribution was helpful to
|
|
| 4/17/2018 5:33 AM | |
|
Posts: 3 Rating:
|
Thank you for your help. |
Follow us on