(0)| 8/19/2008 7:55 AM | |
|
Posts: 12 Rating:
|
Hi, What are the serial communication possibilities with s7-400 hardware (PCS 7 platform) with external devices ? The device (IRCON Maxline 2 Thermal Imager) is claimed to provide a serial RS 485 output through ASCII protocol. Do I need to provide any hardware in S7 (e.g CP 340 /341) for communication ? Does it require additional programming for the communication to take place ?? Does Siemens have any manual for this kind of communication options ? Attachment050915 Rev I p.pdf (426 Downloads) |
| 8/19/2008 9:58 AM | |
|
Joined: 4/6/2006 Last visit: 11/21/2025 Posts: 604 Rating:
|
Hi DJB, Yes you need some additional hardware to communicate over a Serial Protocol. This protocol needs to be programmed too. For the S7-400 you will need to use the CP440/CP441-1/CP441-2. Some usefull information can be found in the 2 manuals and the FAQ available with the links below. Manual Point-to-point Communication CP 440 Installation and Parameter Assignment Manual CP 441 Point-to-Point Commmunication Installation and Parameter Assignment What should you watch out for when receiving data with ASCII drivers via serial S7-300/400 CPs? |
|
Best regards, |
|
Follow us on