(0)| 6/21/2018 11:16 AM | |
|
Posts: 19 Rating:
|
hi I was trying to create a machine backup. By setting up a new PLC at our department for training purpose, but this following error is coming, when i am trying to download the hardware configuration to IM151-8 PN/DP CPU. Download (33:279): The block/op. sys. update is too large. Download (13:4718): Cannot load SDB 7. Download (13:4589): The system data cannot be loaded to module IM151-8 PN/DP CPU - (R0/S2) of station SIMATIC 300(2). Look under details or try to determine the cause for the problem using the diagnostic buffer of the module. Am i missing something? because the machine is having the same setup. Or Is my Simatic manager software is having some problem. please suggest? AttachmentP.zip (506 Downloads) |
| 6/21/2018 11:17 AM | |
|
Joined: 5/12/2006 Last visit: 1/20/2026 Posts: 22829 Rating:
|
Hello, is the PLC in STOP? Christoph |
| 6/21/2018 11:18 AM | |
|
Posts: 19 Rating:
|
thanks for quick response yes PLC is in stop mode and i am not using any memory card. |
| 6/21/2018 11:38 AM | |
|
Joined: 4/24/2006 Last visit: 1/20/2026 Posts: 9106 Rating:
|
Hello, You need a Memory Card. That will be your Load Memory. Best regards, Wizard |
Follow us on