6/20/2018 5:09 PM | |
Posts: 6 Rating: (0) |
Dear Christoph, I have the same problem but not with the simulation it's real system. My old system (It's running ok): PLC: CPU313C Software: Step7 V5.3 WinCC flexible 2008 HMI: TP177A (or TP170) I want to replace the TP177A by the new one TP700 and I used the TIA portal Wincc comport/avandce to migrated and loaded the old program to the new HMI. But when after I loaded the program to the HMI and connect to the PLC. The #### change to 0 (or another number) but the I just change 1 or 2 graphic page, cannot go to the others. Before connected to the PLC I can go to all the graphic page easily. Can you help me. Best regard, Huan ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/21/2018 10:58:27 AMNew subject after splitting |
|
Follow us on