(0)| 7/18/2018 9:26 AM | |
|
Joined: 12/12/2016 Last visit: 12/11/2025 Posts: 640 Rating:
|
Hello! As far as I know there are no mPCIe SSDs available on the market. Most use the mSATA interface which looks just like mPCIe, but its not the same. However, it should be possible to connect a M.2 SSD to the IOT using a mPCIe to M.2 Adapter. This adapter worked for me when I connected an M.2 WIFI card to the IOT. To connect an NVME SSD you would need an adapter that converts to M.2 Key M. But I can't tell for sure if it will work. Kind regards! |
Last edited by: Fe_lipe at: 7/18/2018 9:56:57 AM |
|
Follow us on