(0)| 7/20/2018 11:36 AM | |
|
Posts: 51 Rating:
|
Hi All So i have this setup which is working perfect for calculating machine up time as a live percentage on the HMI with a reset button which is used every 8 hours. However sometimes the machine needs to be turned off in the instance of a fault, when this happens all the data is wiped. Is there anyway of storing this data so it resumes from the same place when the machine is turned back on? AttachmentMITUTOYO FINAL PROGRAM percentage calculator opposite inputs.zip (179 Downloads) |
| 7/20/2018 11:39 AM | |
|
Joined: 12/18/2014 Last visit: 1/20/2026 Posts: 36494 Rating:
|
Which device is switched off? HMI or LOGO! ? |
| 7/20/2018 11:41 AM | |
|
Posts: 51 Rating:
|
The logo, when the machine is turned off the power to the logo is also taken out as it supply's the logo with the 24V |
| 7/20/2018 11:49 AM | |
|
Posts: 51 Rating:
|
So is there any way to retain these values? |
| 7/20/2018 1:45 PM | |
|
Joined: 12/18/2014 Last visit: 1/20/2026 Posts: 36494 Rating:
|
Set the check mark by retentivity. |
Follow us on