(0)| 9/26/2018 8:56 AM | |
|
Posts: 1 Rating:
|
Hello I need urgent help. I am S7 300 PLC user CPU 315-DP. My system have some peripheral I/0 Devices. so here we use profibus DP network. It has 32 station and three IM 153-1 Module. But now the problem is CPU show BF and SF fault. We log in the program and see among 32 station only 13 number station which is IM 153-1 Module shows Bus fault So we Change The profibus cable, Bus connector and also the IM 153-1 module . But after doing all this, problem is still exist then we Diagnostics The module then show a massage like Device Is Not Available Please Help us what should we have to do. ------------------------------------------------------------------------------------------ |
Last edited by: tnvr at: 9/26/2018 8:59:17 AMLast edited by: The Helping Hand at: 9/27/2018 12:55:38 PMNew subject after splitting |
|
| 9/27/2018 4:24 PM | |
|
Posts: 199 Rating:
|
Hi, Send the diagnostic Buffer content, further information within the diagnostic buffer can help you to solve the problem. The replaced card IM153-1 must be the same as the old one otherwise the Hardware Configuration shall be reload with the new configuration. Also you can check the switch of the profibus cable in case the switch is on the resistor position then the bus is cut off. Regards |
Follow us on