(0)| 10/6/2018 11:00 AM | |
|
Joined: 7/21/2018 Last visit: 10/10/2024 Posts: 1 Rating:
|
Hello I want aGSD FILE ET200U 6ES5 318-8MB12.6ES5 318-8MB13Connect with PLC S7400 Software TIA V13 help me please.
Best Reguard, Mr.Ittichai chamchuen(M) Supervisor Automation Beer Thip Brewery (1991) Co.,Ltd
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/8/2018 9:37:21 AMNew subject after splitting Last edited by: The Helping Hand at: 10/8/2018 9:38:19 AMDeleted email adress. |
|
| 10/6/2018 3:10 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Ittichai; First, check in the Profibus catalog (available Profibus slaves, in the Profibus configurator of TIA Portal) whether these ET 200U interface modules are not already available for use, under Distributed IO, Profibus, for example.. If you cannot find them, use the link provided by Wizard earlier, to download and integrate the ET 200S DP file in the Profibus configurator. The following FAQ should give you hints about the integration of a GSD file in TIA Portal: https://support.industry.siemens.com/cs/ww/en/view/109738401 Hope this helps, |
| 10/7/2018 3:11 AM | |
|
Joined: 10/7/2005 Last visit: 1/20/2026 Posts: 3054 Rating:
|
Have a look at the FAQ Coupling ET200U DP (6ES5 318 8MB12) to an S7 master too, as DIP switch 8 needs to set correctly to make it work. |
|
Cheers |
|
This contribution was helpful to
|
|
Follow us on