(0)| 10/18/2018 8:10 PM | |
|
Posts: 1 Rating:
|
I'm having trouble reading and writing to a db via s7 connected between iot2000 (nodered) and cpu1212c. This is all configured I can read and write in the IO's and memories, but in the DB's it does not give any signal. this is my nodes: [{"id":"f81032d5.d951f","type":"inject","z":"f26856cb.bd8408","name":"TRUE","topic":"","payload":"true","payloadType":"bool","repeat":"","crontab":"","once":false,"onceDelay":0.1,"x":1650,"y":160,"wires":[["20ea24ac.b414ac"]]},{"id":"3e116873.e73dd8","type":"inject","z":"f26856cb.bd8408","name":"FALSE","topic":"","payload":"false","payloadType":"bool","repeat":"","crontab":"","once":false,"onceDelay":0.1,"x":1650,"y":220,"wires":[["20ea24ac.b414ac"]]},{"id":"283f8645.f9dc1a","type":"comment","z":"f26856cb.bd8408","name":"ACIONA DB","info":"","x":1650,"y":100,"wires":[]},{"id":"2f880281.1b9cde","type":"debug","z":"f26856cb.bd8408","name":"RECEBE BOOL","active":true,"tosidebar":true,"console":false,"tostatus":false,"complete":"payload","x":1860,"y":340,"wires":[]},{"id":"5fa11a84.a83f84","type":"s7 in","z":"f26856cb.bd8408","endpoint":"ffb2be5.b5ba44","mode":"single","variable":"testiculo","diff":true,"name":"DB1.DBX0.0","x":1650,"y":340,"wires":[["2f880281.1b9cde"]]},{"id":"96530b25.02db28","type":"comment","z":"f26856cb.bd8408","name":"MONITORA DB","info":"","x":1660,"y":280,"wires":[]},{"id":"20ea24ac.b414ac","type":"s7 out","z":"f26856cb.bd8408","endpoint":"ffb2be5.b5ba44","variable":"testiculo","name":"DB1.DBX0.0","x":1890,"y":180,"wires":[]},{"id":"ffb2be5.b5ba44","type":"s7 endpoint","z":"f26856cb.bd8408","address":"192.168.200.101","port":"102","rack":"0","slot":"1","localtsaphi":"01","localtsaplo":"00","remotetsaphi":"01","remotetsaplo":"00","connmode":"rack-slot","cycletime":"500","timeout":"1500","verbose":"default","name":"CPU 1212C","vartable":[{"addr":"Q0.0","name":"QLF-DC-CIRC-01"},{"addr":"I0.0","name":"QTA-161"},{"addr":"DB10.DBX0.0","name":"LERBOOL"},{"addr":"DB10.DBD4","name":"LERREAL"},{"addr":"DB10.DBW2","name":"LERWORD"},{"addr":"M4.0","name":"TESTEDEMEM"},{"addr":"DB1.DBX0.0","name":"testiculo"}]}] ------------------------------------------------------------------------------------------ |
Last edited by: MAFS at: 10/18/2018 8:12:42 PMLast edited by: Jen_Moderator at: 10/19/2018 10:49:29 AMNew subject after splitting |
|
Follow us on