(0)| 10/11/2018 6:05 PM | |
|
Joined: 12/15/2006 Last visit: 11/5/2025 Posts: 50 Rating:
|
Hi all, I have: - 1 BR PLC with OPC UA - 1 S7-1512F with OPC UA - 1 Laptop with OPC UAExpert - 1 Laptop with OPC UAExpert / TP2200 (simulated) with TIA V15 Comfort The UAexport on both Laptops can connect to both the BR and Siemens PLC's! The "TP2200 (simulated) with TIA V15 Comfort" Laptop can connect with the Siemens PLC but not with the BR System. I have tried the BR System with both absolute IP addressing (192.168.254.XXX) and symbolic addressing \\WIN-PV40... that the "Simulated TP2200" in the Setup connection area can see(<--?). security is OFF(None) Need help. thank you |
| 11/28/2018 1:16 PM | |
|
Posts: 1 Rating:
|
Any progress? Did you get it working in the end? I'm having problems connecting with the B&R PLC's OPC UA server as well. |
Follow us on