(0)| 12/24/2018 6:17 AM | |
|
Posts: 27 Rating:
|
Dear All, HMI: KTP 700 Baic, PLC, S7 1200 CPU HMI Connections: 4 Functionality: When user click on any button on HMI (Event setbit, M2.6), then screen will move to Screen num 3 using Job mail box in PLC ladder. PFA zip file. But when I click button on HMI (Event setbit, M2.6), the conditions in that rungs gets works well like ADD, SUB, Timer ON,SET, RESET but values in MW800 (Jobmailbox) & MW802 not get move sometimes. So that screen not get switch. Sometimes it moves. This I cause repetitive click on HMI. Please anybody have solution pls suggest. AttachmentHMI Jobmailbox.zip (175 Downloads) |
| 12/24/2018 8:42 AM | |
|
Posts: 2826 Rating:
|
What is the acquisition cycle (update rate) like? What happens when the rate is set to 100ms? |
This contribution was helpful to
|
|
| 12/24/2018 9:59 AM | |
|
Posts: 27 Rating:
|
Thank you #dP It is by default 1 second. If I change it to '100 ms', will it eliminate the issue? |
Follow us on