(0)| 1/15/2019 8:12 AM | |
|
Joined: 4/28/2015 Last visit: 1/15/2026 Posts: 3345 Rating:
|
Hi, are these 6 sensors Modbus TCP or Modbus RTU? I have never tried to use the IOT2000 with a battery as power supply. You can use supply voltage from 9 - 36V DC, with 24V the IOT2000 has a power consumtion of 3,5W without any devices plugged. You can find more electrical information in the technical data section of the manual. If you find a suitable battery this should work I think. The IOT2000 can store the data, e.g in a file or a database. You can use SD cards from 2GB up top 32GB and use all the available storage space on the SD card to store data. If you store this in a file you could easily copy the file from the IOT2000 to your laptop using WinSCP. This has to be done manually. I hope this helps! If it is not clear, just ask Best regards! |
|
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on