(0)| 2/1/2019 9:58 PM | |
|
Posts: 4 Rating:
|
Thanks for your reply, Exactly, is it possible to use a simple logo to control the frequency and direction of two motors alternately, or should I go for a PLC. |
| 2/3/2019 3:34 AM | |
|
Posts: 1283 Rating:
|
I would suggest you use TIA Online Selection Tool that will help you to guide through the whole selection process regarding controllers and Drives. Also you can select software for engineering and export the list to Excel as well. I would suggest you evaluate the number of Digital IO and Analog IO for your project. Make a list and select controllers based on that. If you want to read all the parameters of the Drive to HMI display, you can make use of PROFINET communication which can be selected for the drives. You can get S7-1200 Series PLC and select different CPU based on your requirement and you can integrate your Drive easily with this PLC using PROFINET. Thanks, Jay |
| 2/3/2019 10:45 PM | |
|
Posts: 4 Rating:
|
Thank You very much Jay |
Follow us on